IPxi::BusNumber

Description

Returns the PCI bus number.

VB Prototype

Dim value As Short
value = object.BusNumber

C++ Prototype

HRESULT get_BusNumber(
  short* BusNumber
);

Return Value

Refer to the table of return codes.

See Also

ActualLinkWidth, BusNumber, ChassisNumber, Close, ComponentVersion, DevNumber, DstarBusNumber, DstarLineSet, FuncNumber, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, Init, IsExpress, LastStatus, LockRsrc, LockState, MaxLinkWidth, MemBaseBar0, MemBaseBar1, MemBaseBar2, MemBaseBar3, MemBaseBar4, MemBaseBar5, MemSizeBar0, MemSizeBar1, MemSizeBar2, MemSizeBar3, MemSizeBar4, MemSizeBar5, MemTypeBar0, MemTypeBar1, MemTypeBar2, MemTypeBar3, MemTypeBar4, MemTypeBar5, OptionString, ProgID, ResourceName, SessionType, SlotLinkWidth, SlotLocalBusLeft, SlotLocalBusRight, SlotPath, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, SpecVersion, StarTriggerBus, StarTriggerLine, Timeout, TriggerBus, UnlockRsrc, IPxi Overview