IPxi::StarTriggerBus
Description
Returns a value indicating the PXI star trigger bus.
VB Prototype
Dim value As Short
value = object.StarTriggerBus
C++ Prototype
HRESULT get_StarTriggerBus(
short* StarTriggerBus
);
Return Value
Refer to the table of return codes.
See Also
ActualLinkWidth, BusNumber, ChassisNumber, Close, ComponentVersion, DevNumber, DstarBusNumber, DstarLineSet, FuncNumber, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, Init, IsExpress, LastStatus, LockRsrc, LockState, MaxLinkWidth, MemBaseBar0, MemBaseBar1, MemBaseBar2, MemBaseBar3, MemBaseBar4, MemBaseBar5, MemSizeBar0, MemSizeBar1, MemSizeBar2, MemSizeBar3, MemSizeBar4, MemSizeBar5, MemTypeBar0, MemTypeBar1, MemTypeBar2, MemTypeBar3, MemTypeBar4, MemTypeBar5, OptionString, ProgID, ResourceName, SessionType, SlotLinkWidth, SlotLocalBusLeft, SlotLocalBusRight, SlotPath, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, SpecVersion, StarTriggerBus, StarTriggerLine, Timeout, TriggerBus, UnlockRsrc, IPxi Overview