IPxi::FuncNumber

Description

Returns the PCI function number.

VB Prototype

Dim value As Short
value = object.FuncNumber

C++ Prototype

HRESULT get_FuncNumber(
  short* FuncNumber
);

Return Value

Refer to the table of return codes.

See Also

ActualLinkWidth, BusNumber, ChassisNumber, Close, ComponentVersion, DevNumber, DstarBusNumber, DstarLineSet, FuncNumber, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, Init, IsExpress, LastStatus, LockRsrc, LockState, MaxLinkWidth, MemBaseBar0, MemBaseBar1, MemBaseBar2, MemBaseBar3, MemBaseBar4, MemBaseBar5, MemSizeBar0, MemSizeBar1, MemSizeBar2, MemSizeBar3, MemSizeBar4, MemSizeBar5, MemTypeBar0, MemTypeBar1, MemTypeBar2, MemTypeBar3, MemTypeBar4, MemTypeBar5, OptionString, ProgID, ResourceName, SessionType, SlotLinkWidth, SlotLocalBusLeft, SlotLocalBusRight, SlotPath, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, SpecVersion, StarTriggerBus, StarTriggerLine, Timeout, TriggerBus, UnlockRsrc, IPxi Overview