ISharedRegister::ComponentVersion

Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.

Description

A numeric version for this component.

VB Prototype

Dim value As Long
value = object.ComponentVersion

C++ Prototype

HRESULT get_ComponentVersion(
  long* ComponentVersion
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AllocateMemory, FreeMemory, ISharedRegister Overview