ISharedRegister::GetAttribute
Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.
Description
Use of this method is discouraged. All the non-deprecated standard attributes are accessible via properties on the appropriate COM interfaces.
VB Prototype
value As
Variant = GetAttribute(
attribute As Long
)
C++ Prototype
HRESULT GetAttribute(
long attribute,
VARIANT* pAttrState
);
Parameters
attribute
The attribute type to retrieve.
pAttrState
The value of the attribute.
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AllocateMemory, FreeMemory, ISharedRegister Overview