ISharedRegister::LastStatus

Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.

Description

The return value from the last method call on this interface. This property may be useful in Visual Basic, where positive return values, such as warnings and other non-error return values, cannot be retrieved.

See the Return Values page for a list of positive return values.

VB Prototype

Dim value As HRESULT
value = object.LastStatus

C++ Prototype

HRESULT get_LastStatus(
  HRESULT* LastStatus
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AllocateMemory, FreeMemory, ISharedRegister Overview