ITcpipInstr::HardwareInterfaceName
Description
The name of the hardware interface (GPIB, ASRL, etc.).
VB Prototype
Dim value As String
                                            value = object.HardwareInterfaceName
                                        
C++ Prototype
HRESULT get_HardwareInterfaceName(
                                        
  BSTR* HardwareInterfaceName
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, Address, HostName, DeviceName, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, ITcpipInstr Overview