ITcpipInstr::UnlockRsrc
Description
Unlocks the resource
VB Prototype
UnlockRsrc(
                                        
)
	
C++ Prototype
HRESULT UnlockRsrc(
                                        
);
	
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, Address, HostName, DeviceName, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, ITcpipInstr Overview