ITcpipInstr::HostName
Description
Specifies the host name of the device. If no host name is available, this attribute returns an empty string.
VB Prototype
Dim value As String
                                            value = object.HostName
                                        
C++ Prototype
HRESULT get_HostName(
                                        
  BSTR* HostName
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, Address, HostName, DeviceName, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, ITcpipInstr Overview