IVisaSession::ComponentVersion
Description
A numeric version for this component.
VB Prototype
Dim value As Long
                                            value = object.ComponentVersion
                                        
C++ Prototype
HRESULT get_ComponentVersion(
                                        
  long* ComponentVersion
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, IVisaSession Overview