IVisaSession::LockState
Description
The current locking state of the interface.
VB Prototype
Dim value As AccessMode
                                            value = object.LockState
                                        
C++ Prototype
HRESULT get_LockState(
                                        
  AccessMode* LockState
);
		
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, IVisaSession Overview