IVisaSession::OptionString

Description

The option string corresponding to the current state of the resource.

See The Option String for more information on the option string property.

VB Prototype

Dim value As String
value = object.OptionString

C++ Prototype

HRESULT get_OptionString(
  BSTR* OptionString
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, IVisaSession Overview