IVxiBackplane::MainframeLA

Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.

Description

Logical address of a given device in the mainframe, usually the device with the lowest logical address.  Other possible values include the logical address of the slot-0 controller or of the parent-side extender.  Often, these are all the same value.  The purpose of this attribute is to provide a unique ID for each mainframe.  A VISA manufacturer can choose any of these values, but must be consistent across mainframes.  If this value is not known, the attribute value returned is UNKNOWN_LA.

VB Prototype

Dim value As Short
value = object.MainframeLA

C++ Prototype

HRESULT get_MainframeLA(
  short* MainframeLA
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, MainframeLA, TriggerID, TriggerStatus, TriggerSupport, VxiVmeInterruptStatus, VxiVmeSysfailStatus, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertInterruptSignal, AssertTrigger, AssertUtilSignal, MapTrigger, UnmapTrigger, IVxiBackplane Overview