IVxiBackplane::VxiVmeInterruptStatus
Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.
Description
Shows the current state of the VXI/VME interrupt lines. This is a bit vector with bits 0-6 corresponding to interrupt lines 1-7.
VB Prototype
Dim value As Short
value = object.VxiVmeInterruptStatus
C++ Prototype
HRESULT get_VxiVmeInterruptStatus(
short* VxiVmeInterruptStatus
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, MainframeLA, TriggerID, TriggerStatus, TriggerSupport, VxiVmeInterruptStatus, VxiVmeSysfailStatus, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertInterruptSignal, AssertTrigger, AssertUtilSignal, MapTrigger, UnmapTrigger, IVxiBackplane Overview