IVxiBackplane::TriggerStatus

Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.

Description

Shows the current state of the VXI trigger lines.  This is a bit vector with bits 0-9 corresponding to TRIG_TTL0 through TRIG_ECL1.

VB Prototype

Dim value As Long
value = object.TriggerStatus

C++ Prototype

HRESULT get_TriggerStatus(
  long* TriggerStatus
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, MainframeLA, TriggerID, TriggerStatus, TriggerSupport, VxiVmeInterruptStatus, VxiVmeSysfailStatus, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AssertInterruptSignal, AssertTrigger, AssertUtilSignal, MapTrigger, UnmapTrigger, IVxiBackplane Overview