Keysight VISA.NET Help
IMessageBasedRawIO Interface
Members 



The IMessageBasedRawIO interface includes methods that read and write data to/from a device without trying to format or parse it. It also is capable of performing asynchronous I/O reads and writes with a flexible set of mechanisms for notifying the calling program that the asynchronous I/O operation is complete.

For more information, see Raw I/O.

Syntax
'Declaration
 
Public Interface IMessageBasedRawIO 
'Usage
 
Dim instance As IMessageBasedRawIO
public interface IMessageBasedRawIO 
public interface class IMessageBasedRawIO 
Requirements

Current with Keysight IO Libraries Suite 18

See Also

Reference

IMessageBasedRawIO Members
Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025