Keysight VISA.NET Help
IMessageBasedRawIO Interface Members
Methods 

The following tables list the members exposed by IMessageBasedRawIO.

Public Methods
 NameDescription
 MethodAbortAsyncOperation Requests the session to terminate normal execution of an asynchronous read or write operation.  
 MethodBeginReadOverloaded. Read count bytes asynchronously and store them in the Async Results Buffer/>.  
 MethodBeginWriteOverloaded. Write the buffer to the device asynchronously.  
 MethodEndRead Clean up resources created and used as part of the asynchronous read operation.  
 MethodEndReadString Clean up resources created and used as part of the asynchronous read operation and return the string that was read.  
 MethodEndWrite Clean up resources created and used as part of the asynchronous write operation.  
 MethodReadOverloaded.  Read bytes until an END indicator or termination character is reached.  
 MethodReadStringOverloaded.  Read characters into the return string until an END indicator or termination character is reached.  
 MethodWriteOverloaded. Write buffer to the device.  
Top
See Also

Reference

IMessageBasedRawIO Interface
Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025