Keysight VISA.NET Help
ReadString Method (IMessageBasedRawIO)



Read characters into the return string until an END indicator or termination character is reached.
Overload List
OverloadDescription
ReadString() Read characters into the return string until an END indicator or termination character is reached.  
ReadString(Int64)Read count characters into the return string, or until an END indicator or termination character is reached, whichever comes first.  
ReadString(Int64,ReadStatus)Read count characters into the return string, or until an END indicator or termination character is reached, whichever comes first.  
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025