Keysight VISA.NET Help
IVxiBackplaneSession Interface Properties

For a list of all members of this type, see IVxiBackplaneSession members.

Public Properties
 NameDescription
 PropertyChassisLogicalAddress The logical address of a given device in the mainframe that serves as a unique ID for the mainframe  
 PropertyEventQueueCapacity The capacity of the event queue - the maximum number of pending events. (Inherited from Ivi.Visa.IVisaSession)
 PropertyHardwareInterfaceName Human readable text that describes the hardware interface. (Inherited from Ivi.Visa.IVisaSession)
 PropertyHardwareInterfaceNumber The board number of the hardware interface. (Inherited from Ivi.Visa.IVisaSession)
 PropertyHardwareInterfaceType Specifies the hardware interface type (GPIB, ASRL, etc.). (Inherited from Ivi.Visa.IVisaSession)
 PropertyInterruptStatus The current state of the VXI/VME interrupt lines.  
 PropertyResourceClass The class of resource for this session (INSTR, INTFC, etc.). (Inherited from Ivi.Visa.IVisaSession)
 PropertyResourceImplementationVersion The version of this VISA.NET implementation. (Inherited from Ivi.Visa.IVisaSession)
 PropertyResourceLockState The current lock state of the resource for this session. (Inherited from Ivi.Visa.IVisaSession)
 PropertyResourceManufacturerId The IVI identification number of the software vendor of this VISA.NET implementation. (Inherited from Ivi.Visa.IVisaSession)
 PropertyResourceManufacturerName The name of the software vendor that corresponds to the ResourceManufacturerId property. (Inherited from Ivi.Visa.IVisaSession)
 PropertyResourceName The VISA resource name of the currently open resource. This name is the canonical version of the resource name and therefore may vary from the resource descriptor used to open/initialize the resource. (Inherited from Ivi.Visa.IVisaSession)
 PropertyResourceSpecificationVersion The version of the VISA.NET specification that describes the functionality provided by this session. (Inherited from Ivi.Visa.IVisaSession)
 PropertySynchronizeCallbacks Specifies whether callbacks must be performed in a specific synchronization context. If false, the implementation is allowed to execute callbacks in any context. The default value is true. (Inherited from Ivi.Visa.IVisaSession)
 PropertySystemFailureStatus The current state of the VXI/VME SYSFAIL (SYStem FAILure) backplane line.  
 PropertyTimeoutMilliseconds The I/O timeout in milliseconds for I/O communication on this resource session. If the timeout is VisaConstants.ImmediateTimeout (0), operations will never wait for the device to respond. If the timeout is VisaConstants.InfiniteTimeout (-1), I/O communication will not timeout. (Inherited from Ivi.Visa.IVisaSession)
 PropertyTriggerStatus The VXI trigger line(s) that are currently set.  
 PropertyTriggerSupport The VXI trigger line(s) that this implementation supports.  
Top
See Also

Reference

IVxiBackplaneSession Interface
Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025