Keysight VISA.NET Help
IVxiMemorySession Interface Members
Properties  Methods 

The following tables list the members exposed by IVxiMemorySession.

Public Properties
 NameDescription
 PropertyAllowDma Specifies whether direct memory access is enabled. In some cases you may not be able to change whether DMA is enabled, so reading this property value may not return the same value that was set. (Inherited from Ivi.Visa.IRegisterBasedSession)
 PropertyDestinationIncrement For MoveOut methods, specifies whether to do a block move or a FIFO write. (Inherited from Ivi.Visa.IRegisterBasedSession)
 PropertyEventQueueCapacity The capacity of the event queue - the maximum number of pending events. (Inherited from Ivi.Visa.IVisaSession)
 PropertyHardwareInterfaceName Human readable text that describes the hardware interface. (Inherited from Ivi.Visa.IVisaSession)
 PropertyHardwareInterfaceNumber The board number of the hardware interface. (Inherited from Ivi.Visa.IVisaSession)
 PropertyHardwareInterfaceType Specifies the hardware interface type (GPIB, ASRL, etc.). (Inherited from Ivi.Visa.IVisaSession)
 PropertyLogicalAddress The logical address of the VXI or VME controller for this interface.  
 PropertyResourceClass The class of resource for this session (INSTR, INTFC, etc.). (Inherited from Ivi.Visa.IVisaSession)
 PropertyResourceImplementationVersion The version of this VISA.NET implementation. (Inherited from Ivi.Visa.IVisaSession)
 PropertyResourceLockState The current lock state of the resource for this session. (Inherited from Ivi.Visa.IVisaSession)
 PropertyResourceManufacturerId The IVI identification number of the software vendor of this VISA.NET implementation. (Inherited from Ivi.Visa.IVisaSession)
 PropertyResourceManufacturerName The name of the software vendor that corresponds to the ResourceManufacturerId property. (Inherited from Ivi.Visa.IVisaSession)
 PropertyResourceName The VISA resource name of the currently open resource. This name is the canonical version of the resource name and therefore may vary from the resource descriptor used to open/initialize the resource. (Inherited from Ivi.Visa.IVisaSession)
 PropertyResourceSpecificationVersion The version of the VISA.NET specification that describes the functionality provided by this session. (Inherited from Ivi.Visa.IVisaSession)
 PropertySourceIncrement For MoveIn methods, specifies whether to do a block move or a FIFO read. (Inherited from Ivi.Visa.IRegisterBasedSession)
 PropertySynchronizeCallbacks Specifies whether callbacks must be performed in a specific synchronization context. If false, the implementation is allowed to execute callbacks in any context. The default value is true. (Inherited from Ivi.Visa.IVisaSession)
 PropertyTimeoutMilliseconds The I/O timeout in milliseconds for I/O communication on this resource session. If the timeout is VisaConstants.ImmediateTimeout (0), operations will never wait for the device to respond. If the timeout is VisaConstants.InfiniteTimeout (-1), I/O communication will not timeout. (Inherited from Ivi.Visa.IVisaSession)
Top
Public Methods
 NameDescription
 MethodDisableEventDisables a client from receiving events of type(s) specified by the eventType argument. (Inherited from Ivi.Visa.IVisaSession)
 MethodDiscardEventsDiscard all pending events of type(s) specified by the eventType argument. (Inherited from Ivi.Visa.IVisaSession)
 MethodDispose (Inherited from System.IDisposable)
 MethodEnableEventEnables a client to receive events of the type specified by the eventType argument using a WaitOnEvent method. (Inherited from Ivi.Visa.IVisaSession)
 MethodIn16 Read in a 16-bit value from the specified memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession)
 MethodIn32 Read in a 32-bit value from the specified memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession)
 MethodIn64 Read in a 64-bit value from the specified memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession)
 MethodIn8 Read in an 8-bit value from the specified memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession)
 MethodLockResource Locks the resource for this session with an exclusive lock, with an infinite timeout. (Inherited from Ivi.Visa.IVisaSession)
 MethodMapAddress Map the specified memory space into this process’s address space. (Inherited from Ivi.Visa.IRegisterBasedSession)
 MethodMove Moves data from the specified source to the specified destination.  
 MethodMoveIn16 Move a 16-bit block of data from the specified memory space (assigned memory base + offset) to local memory. (Inherited from Ivi.Visa.IRegisterBasedSession)
 MethodMoveIn32 Move a 32-bit block of data from the specified memory space (assigned memory base + offset) to local memory. (Inherited from Ivi.Visa.IRegisterBasedSession)
 MethodMoveIn64 Move a 64-bit block of data from the specified memory space (assigned memory base + offset) to local memory. (Inherited from Ivi.Visa.IRegisterBasedSession)
 MethodMoveIn8 Move an 8-bit block of data from the specified memory space (assigned memory base + offset) to local memory. (Inherited from Ivi.Visa.IRegisterBasedSession)
 MethodMoveOut16 Moves an 16-bit block of data from local (source) memory to the specified destination memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession)
 MethodMoveOut32 Moves an 32-bit block of data from local (source) memory to the specified destination memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession)
 MethodMoveOut64 Moves an 64-bit block of data from local (source) memory to the specified destination memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession)
 MethodMoveOut8 Moves an 8-bit block of data from local (source) memory to the specified destination memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession)
 MethodOut16 Write a 16-bit value to the specified memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession)
 MethodOut32 Write a 32-bit value to the specified memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession)
 MethodOut64 Write a 64-bit value to the specified memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession)
 MethodOut8 Write an 8-bit value to the specified memory space (assigned memory base + offset). (Inherited from Ivi.Visa.IRegisterBasedSession)
 MethodUnlockResource Unlock the resource. (Inherited from Ivi.Visa.IVisaSession)
 MethodWaitOnEventWait for events of type(s) specified by the eventType argument. (Inherited from Ivi.Visa.IVisaSession)
Top
See Also

Reference

IVxiMemorySession Interface
Ivi.Visa Namespace

 

 


© Keysight Technologies 2015-2025