viMapTrigger

This section contains information specific to the Windows product.

Syntax

viMapTrigger(ViSession vi, ViInt16 trigSrc, ViInt16 trigDest, ViUInt16 mode);

Description

Map the specified trigger source line to the specified destination line. This operation can be used to map one trigger line to another. This operation is valid only on Backplane (BACKPLANE) sessions.

If this operation is called multiple times on the same BACKPLANE resource with the same source trigger line and different destination trigger lines, the result should be that when the source trigger line is asserted all specified destination trigger lines should also be asserted.

If this operation is called multiple times on the same BACKPLANE resource with different source trigger lines and the same destination trigger line the result should be that when any of the specified source trigger lines is asserted, the destination trigger line should also be asserted.

However, mapping a trigger line (as either source or destination) multiple times requires special hardware capabilities and is not guaranteed to be implemented.

Mapping one trigger line to another modifies the state of hardware. Therefore, the effect continues beyond the scope of the VISA session that mapped it, even if that VISA session is closed.

Parameters

Name

Dir

Type

Description

vi

IN

ViSession

Unique logical identifier to a session.

trigSrc

IN

ViInt16

Source line from which to map.

trigDest

IN

ViInt16

Destination line to which to map.

mode

IN

ViUInt16

Specifies the trigger mapping mode. This should always be VI_NULL for VISA 3.0 and later.

Special Values for trgSrc and trigDest Parameters

Value

 

 

Action Description

VI_TRIG_ECL0 - VI_TRIG_ECL1

 

 

Map the specified VXI ECL trigger line.

VI_TRIG_PANEL_IN

 

 

Map the controller's front panel trigger input line.

VI_TRIG_PANEL_OUT

 

 

Map the controller's front panel trigger output line.

VI_TRIG_STAR_SLOT1 - VI_TRIG_STAR_SLOT12

 

 

Map the specified STAR input trigger line.

VI_TRIG_STAR_VXI0 - VI_TRIG_STAR_VXI2

 

 

Map the specified STAR trigger output line.

VI_TRIG_TTL0 - VI_TRIG_TTL11

 

 

Map the specified TTL trigger line.

Return Values

Type ViStatus

This is the function return status. It returns either a completion code or an error code as follows.

Completion Code

Description

VI_SUCCESS

Operation completed successfully.

VI_SUCCESS_TRIG_MAPPED

The path from trigSrc to trigDest is already mapped.

Error Code

Description

VI_ERROR_INV_LINE

One of the specified lines (trigSrc or trigDest) is invalid.

VI_ERROR_INV_MODE

The value specified by the mode parameter is invalid.

VI_ERROR_INV_SESSION
VI_ERROR_INV_OBJECT

The given session or object reference is invalid (both are the same value).

VI_ERROR_LINE_IN_USE

One of the specified lines (trigSrc or trigDest) is currently in use.

VI_ERROR_NSUP_LINE

One of the specified lines (trigSrc or trigDest) is not supported by this VISA implementation.

VI_ERROR_NSUP_OPER

The given vi does not support this operation.

VI_ERROR_RSRC_LOCKED

Specified operation could not be performed because the resource identified by vi has been locked for this kind of access.

VI_ERROR_TMO

viMapAddress could not acquire resource or perform mapping before the timer expired.

See Also

BACKPLANE Resource Description