Remote USB Interface
A remote USB interface is a device on a LAN that provides connectivity to instruments via USB. It is typically either a gateway, such as the Keysight E5810B LAN/GPIB/USB Gateway, or a computer running the Remote IO Server software.
Remote USB Interface Properties
Property | Description |
---|---|
VISA Interface ID | A name that Keysight software and VISA use to uniquely identify this remote interface.The format of the VISA interface ID for a remote USB interface is USBn, where n is an integer. |
TCPIP Interface ID | The PC's LAN interface to connect to the remote interface over the LAN. See Add a LAN Interface for more information. |
Find Interfaces | If the remote interface you want to use is connected to your local subnet, click Find Interfaces to search for the remote interface using common remote interface names. Select the interface you want to use. The hostname or IP address and the interface name are filled in on the selected remote interface. |
Hostname or IP Address |
|
SICL Interface Name on Remote Host | If you use the Find Interfaces button to select an interface, this field will be filled in for you. Otherwise, enter the SICL interface ID for the remote interface in the Interface name on the remote host field (for example, usb0). |
Verify Connection |
|