ISharedRegister64::FreeMemory

Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.

Description

Frees the memory previously allocated using AllocateMemory.

VB Prototype

FreeMemory(
  offset As Long
)

C++ Prototype

HRESULT FreeMemory(
  long offset
);

Parameters

offset

Specifies the memory previously allocated with AllocateMemory.

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AllocateMemory, FreeMemory, AllocateMemoryEx, FreeMemoryEx, ISharedRegister64 Overview