ISharedRegister64::SoftwareManufacturerName

Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.

Description

The name of the vendor of this software component.

VB Prototype

Dim value As String
value = object.SoftwareManufacturerName

C++ Prototype

HRESULT get_SoftwareManufacturerName(
  BSTR* SoftwareManufacturerName
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AllocateMemory, FreeMemory, AllocateMemoryEx, FreeMemoryEx, ISharedRegister64 Overview