ISharedRegister64::UnlockRsrc

Note: Keysight's VISA COM does not support a COM server for VXI. The IVxi-related interfaces are listed in this help file because they are included in the global VISA COM library.

Description

Unlocks the resource

VB Prototype

UnlockRsrc(
)

C++ Prototype

HRESULT UnlockRsrc(
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, AllocateMemory, FreeMemory, AllocateMemoryEx, FreeMemoryEx, AllocateMemoryEx, FreeMemoryEx, ISharedRegister64 Overview