ITcpipInstr2::ServerCertificate
Description
Returns the full text of the server certificate in the RFC 5652 PEM format.
VB Prototype
Dim value As String
                                            value = object.ServerCertificate
                                        
C++ Prototype
HRESULT get_ServerCertificate(
                                        
  BSTR* ServerCertificate
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, DeviceName, GetAttribute, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, IsHislip, LastStatus, LockRsrc, LockState, OptionString, ProgID, ResourceName, SaslMechanism, ServerCertificate, ServerCertificateExpirationDate, ServerCertificateIsPerpetual, ServerCertificateIssuerName, ServerCertificateSubjectName, SessionType, SetAttribute, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, TlsCipherSuite , UnlockRsrc, , ITcpipInstr2 Overview