ITcpipInstr2::ServerCertificateIsPerpetual
Description
Returns a value indicating whether the server certificate is perpetual or not.
VB Prototype
Dim value As Boolean
                                            value = object.ServerCertificateIsPerpetual
                                        
C++ Prototype
HRESULT get_ServerCertificateIsPerpetual(
                                        
  VARIANT_BOOL* ServerCertificateIsPerpetual
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, DeviceName, GetAttribute, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, IsHislip, LastStatus, LockRsrc, LockState, OptionString, ProgID, ResourceName, SaslMechanism, ServerCertificate, ServerCertificateExpirationDate, ServerCertificateIsPerpetual, ServerCertificateIssuerName, ServerCertificateSubjectName, SessionType, SetAttribute, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, TlsCipherSuite , UnlockRsrc, , ITcpipInstr2 Overview