ITcpipInstr2::ServerCertificateIssuerName

Description

Returns the issuer name of the server certificate.

VB Prototype

Dim value As String
value = object.ServerCertificateIssuerName

C++ Prototype

HRESULT get_ServerCertificateIssuerName(
  BSTR* ServerCertificateIssuerName
);

Return Value

Refer to the table of return codes.

See Also

Address, Close, ComponentVersion, DeviceName, GetAttribute, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, IsHislip, LastStatus, LockRsrc, LockState, OptionString, ProgID, ResourceName, SaslMechanism, ServerCertificate, ServerCertificateExpirationDate, ServerCertificateIsPerpetual, ServerCertificateIssuerName, ServerCertificateSubjectName, SessionType, SetAttribute, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, TlsCipherSuite , UnlockRsrc, , ITcpipInstr2 Overview