ITcpipSocket2::ServerCertificateExpirationDate
Description
Returns the expiration date of the server certificate.
VB Prototype
Dim value As String
                                            value = object.ServerCertificateExpirationDate
                                        
C++ Prototype
HRESULT get_ServerCertificateExpirationDate(
                                        
  BSTR* ServerCertificateExpirationDate
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, Flush,GetAttribute, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, KeepAlive, LockRsrc, LastStatus, , LockState, NoDelay, OptionString, Port, , ProgID, ResourceName, ServerCertificate, ServerCertificateExpirationDate, ServerCertificateIsPerpetual, ServerCertificateIssuerName, ServerCertificateSubjectName, SessionType, SetAttribute, SetBufferSize, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, TlsCipherSuite , UnlockRsrc, ITcpipSocket2 Overview