ITcpipSocket2::TlsCipherSuite

Description

Returns the TLS cipher suite used by the connection.

VB Prototype

Dim value As String
value = object.TlsCipherSuite

C++ Prototype

HRESULT get_TlsCipherSuite(
  BSTR* TlsCipherSuite
);

Return Value

Refer to the table of return codes.

See Also

Address, Close, ComponentVersion, Flush,GetAttribute, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, KeepAlive, LockRsrc, LastStatus, , LockState, NoDelay, OptionString, Port, , ProgID, ResourceName, ServerCertificate, ServerCertificateExpirationDate, ServerCertificateIsPerpetual, ServerCertificateIssuerName, ServerCertificateSubjectName, SessionType, SetAttribute, SetBufferSize, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, TlsCipherSuite , UnlockRsrc, ITcpipSocket2 Overview