ITcpipSocket2::ServerCertificateIssuerName

Description

Returns the issuer name of the server certificate.

VB Prototype

Dim value As String
value = object.ServerCertificateIssuerName

C++ Prototype

HRESULT get_ServerCertificateIssuerName(
  BSTR* ServerCertificateIssuerName
);

Return Value

Refer to the table of return codes.

See Also

Address, Close, ComponentVersion, Flush,GetAttribute, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, KeepAlive, LockRsrc, LastStatus, , LockState, NoDelay, OptionString, Port, , ProgID, ResourceName, ServerCertificate, ServerCertificateExpirationDate, ServerCertificateIsPerpetual, ServerCertificateIssuerName, ServerCertificateSubjectName, SessionType, SetAttribute, SetBufferSize, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, TlsCipherSuite , UnlockRsrc, ITcpipSocket2 Overview