| Keysight.Visa Namespace : GpibInterfaceSession Class |
For a list of all members of this type, see GpibInterfaceSession members.
| Name | Description | |
|---|---|---|
![]() | AssertTrigger | Asserts a software trigger. |
![]() | ControlAtn | Controls the state of the GPIB ATN interface line, and optionally the active controller state of the local interface board. |
![]() | DisableEvent | Disables a calling program's ability to receive events of the type specified by the eventType argument using a VisaSession.WaitOnEvent method (any overload). (Inherited from Keysight.Visa.VisaSession) |
![]() | DiscardEvents | Discards events of the type specified by the eventType argument from the queue for that event type. (Inherited from Keysight.Visa.VisaSession) |
![]() | Dispose | Overloaded. Performs tasks associated with freeing, releasing, or resetting unmanaged VISA resources used by this session. (Inherited from Keysight.Visa.VisaSession) |
![]() | EnableEvent | Enables a calling program's ability to receive events of the type specified by the eventType argument using a WaitOnEvent method. (Inherited from Keysight.Visa.VisaSession) |
![]() | LockResource | Overloaded. Acquires a lock on the resource for this session. (Inherited from Keysight.Visa.VisaSession) |
![]() | PassControl | Overloaded. Tells the GPIB device at the specified address to become controller in charge (CIC). |
![]() | SendCommand | Writes GPIB command bytes on the bus. |
![]() | SendInterfaceClear | Pulses the interface clear line (IFC) for at least 100 microseconds. This operation asserts the IFC line and the local interface becomes controller in charge (CIC). |
![]() | SendRemoteLocalCommand | Controls the state of the GPIB REN interface line and, optionally, the remote/local state of the device. |
![]() | UnlockResource | Unlocks the resource. (Inherited from Keysight.Visa.VisaSession) |
![]() | WaitOnEvent | Overloaded. Waits for an occurrence of the specified event for this session. In particular, WaitOnEvent suspends execution of the thread on which it is called and waits for the specified event indefinitely. (Inherited from Keysight.Visa.VisaSession) |
| Name | Description | |
|---|---|---|
![]() | Finalize | Performs tasks associated with freeing, releasing, or resetting unmanaged VISA resources used by this session. (Inherited from Keysight.Visa.VisaSession) |