Execute RunOrStopApp Function

Below is an example of RunOrStopApp function execution for Run data logging operation via gRPC service.

The AC Source application will start data logging if the bool status is true (no error is detected).

The application user interface above is served as an example only, your application's user interface may not be same as the example.

See Also

gRPC Service

GeneralInstrumentsAPI.proto

PWACAvionicsAPI.proto

PWACImmunityAPI.proto