IF Input Gain Option EXM Adjustment

This adjustment applies to the following models:

This adjustment inputs a calibrated –25 dBm signal into the External IF INPUT port. Then the Amplitude Error is measured at the center frequency and at offset frequencies across the IF Bandwidth. The offset frequencies are nominally spaced in 4 MHz intervals. If Option B40, B85, or B1X is installed, the adjustment is repeated for those paths.

Click here for troubleshooting.

Required Test Equipment

Test Equipment

Model Number1

Microwave Signal Generator #1

PSG Models
(see equipment list)

Power Meter

N1914A

Microwave Power Sensor

N8485A

Microwave Power Splitter

11667B 

Cable, BNC

8120-1840

Cable, coaxial 3.5 mm

11500E

Adapter, 3.5 mm (m) to 3.5 mm (m)

83059A

Adapter, 3.5 mm (f) to 3.5 mm (f)

  • For 3.5 mm source

83059B

Adapter, 2.4 mm (f) to 3.5 mm (f)

  • For 2.4 mm source

11901B

Adapter, 3.5 mm (f) to Type-N (m)

  • 8485A adapter

08485-60005

  1. Refer to the main Required Equipment table for a list of alternative models.

Connection Setups

Power Meter Calibration

 

IF Input Gain Adjustment Setup