This section lists the test equipment needed to run performance tests and adjustments. Models for each test equipment category are given in order of preference. Alternate models are also listed but should be considered a lower priority. Refer to each individual test for specific setup configurations with required cables and adapters.
|
Instrument |
Recommended Model 1 |
Alternative Model 1 |
Use 2 |
|---|---|---|---|
|
Signal Sources |
|||
|
Microwave
|
E8257D
|
PSG 4
|
A, P, T |
|
Microwave
|
E8257D Option 1EA/1EU |
PSG 4 |
P, A |
|
Ultra
Low Noise Reference
|
Wenzel
Associates Inc 5 |
Wenzel
Associates Inc 5 |
P |
|
DC Pulse Generator |
Schwarzbeck IGUU 29186 |
Schwarzbeck IGUU 29166 |
P, A, U |
|
Function Generator |
33622A |
33611A |
A, P |
|
Network Analyzers |
|||
|
Network Analyzer 1 |
N5247B Option 425
|
N5245B1
N5230A/C* *Not allowed in adjustments or utilities. |
P, A, U |
|
Network Analyzer 2 |
E5071C Option 240 |
E5071C Option 280, 440, or 480 |
P |
|
Counters |
|||
|
Frequency Counter |
53230A |
53132A |
P, T |
|
Meters and Power Sensors (See below for calibration service ordering guidelines.) |
|||
|
Digital Multimeter |
3458A |
34470A |
P, T |
|
Power Meter |
N1914A7 |
N1912A |
P, A, U |
|
RF Power Sensor, Type-N8
|
N8482A CFT |
N8482A * *Non H84 sensors will increase measurement uncertainty. |
A, P |
|
RF Power Sensor, Type-N
|
E9304A Option H18 |
|
A, P, U |
|
Microwave Power Sensor,3.5 mm
|
N8485A CFT |
N8485A 8485A9 |
A, P, U |
|
Microwave Power Sensor, 3.5 mm
|
N8485A STD |
None
|
U |
|
Millimeter Power Sensor, 1.85 mm
|
N8488A |
None
|
U |
|
Millimeter Power Sensor, 2.4 mm
|
N8487A CFT |
N8487A 8487A |
A, P, U |
|
Low
Power Microwave Power Sensor
|
8485D |
|
A, P, U |
|
Low Power Millimeter Power Sensor
|
8487D |
|
A, P, U |
|
Standards |
|||
|
Frequency Standard |
Microsemi 5071A-C002 |
HP 5061B Option 004
|
A, P |
|
50
MHz, |
Z5602B Option H51
|
Z5602A Option H51
|
A |
|
Attenuators |
|||
|
3 dB |
8491A Option 003, H33 11 |
8491B Option 003, H33 11 |
P |
|
6 dB |
8491A Option 006, H33 11 |
8491B Option 006, H33 11 |
P |
|
6 dB
|
8493C Option 006 |
|
A |
|
10 dB |
8491A Option 010, H33 11 |
8491B Option 010, H33 11 |
A, P |
|
10 dB |
8493C Option 010 |
|
P |
|
10 dB
|
8490D Option 010 |
|
P |
|
20 dB |
8491A Option 020 |
8491B Option 020 |
A, P |
|
20 dB |
8493C Option 020 |
|
P |
|
30 dB |
11708A |
|
A, P, U |
|
10 dB |
8496G Option 001, H50 |
8496H Option 001, H50 |
P |
|
1 dB |
8494G Option 001, H50 |
8494H Option 001, H50 |
P |
|
Attenuator |
11716A |
|
P |
|
Attenuator Driver |
11713B |
11713A |
P |
|
Terminations |
|||
|
Type-N (m) |
909A Option 012 |
|
P, T |
|
3.5 mm (m)
|
909D |
|
A, P, T |
|
2.4 mm (f)
|
85138B |
901D |
A, P |
|
BNC, 50 Ω |
1250-0207 |
|
P |
|
Miscellaneous Devices |
|||
|
RF Power Splitter, Type-N |
11667A |
|
A, P, U |
|
Microwave Power Splitter, 3.5 mm |
11667B |
|
A, P, U |
|
Millimeter Power Splitter, 2.4 mm
|
11667C |
|
A, P, U |
|
Directional Bridge |
86205A |
|
P |
|
Microwave Directional Coupler |
87300B |
|
P |
|
Millimeter Directional Coupler
|
87301C |
|
P |
|
Hybrid Power Divider
|
87302C |
|
A |
|
Microwave Power Divider
|
11636B |
|
A |
|
Calibration Kits13 |
|||
|
Mechanical Calibration Kit, Type-N14 |
85032F |
85054B |
P |
|
Mechanical Calibration Kit, Type-N14 |
85054B |
85054D |
P |
|
Mechanical Calibration Kit, 3.5 mm14
|
85033E |
85052B |
P |
|
Mechanical Calibration Kit, 3.5 mm14
|
85052B |
85052C |
P |
|
Mechanical Calibration Kit, 2.4 mm
|
85056A |
|
P |
|
E-Cal Kit, Type-N |
N4690D-M0F |
N4690C-M0F N4690B-M0F |
P |
|
E-Cal Kit, 3.5 mm
|
N4691D-M0F |
N4691B-M0F |
P, A, U |
|
E-Cal Kit, 2.4 mm
|
N4693D-M0F |
N4693A-M0F |
P, A, U |
|
Cables |
|||
|
Coaxial cable, 3.5 mm
|
11500E |
8120-4921 |
A, P, U |
|
Coaxial cable, 2.4 mm
|
8120-6164 |
E7342-60005 (Gore 0Z 0CJ 0CK 0360) |
A, P, U |
|
Coaxial cable, 2.4 mm
|
8121-2065 |
E7342-60005 (Gore 0Z 0CJ 0CK 0360) |
A, P, U |
|
Cable, 3.5
mm (f) to PSC-3.5 mm (f)
|
85131E |
85131F |
P |
|
Cable, 2.4
mm (f) to PSC-2.4 mm (f)
|
85133E |
85133F 85133-60016 |
P |
|
Cable, Type-N
|
11500C |
|
A, P, U, T |
|
Cable, BNC
|
8120-1840 |
8120-2582 |
A, P, U, T |
|
Power Sensor Cable
|
11730A |
|
A, P, T |
|
Filters |
|||
|
50 MHz Low Pass Filter |
Telonic
Berkeley |
0955-0306 |
P, T |
|
300 MHz Low Pass Filter
|
Telonic
Berkeley |
0955-0455 |
P |
|
1.8 GHz Low Pass Filter
|
RLC L-1636 |
0955-0491 |
P |
|
5.0 GHz Low Pass Filter |
RLC F-30-5000-RF |
|
P |
|
8.0 GHz Low Pass Filter |
RLC F-30-8000-RF |
|
P |
|
12.4 GHz Low Pass Filter |
RLC F-30-12.4-RF |
|
P |
|
18 GHz Low Pass Filter
|
RLC F-30-18.0-RF |
|
P |
|
18 MHz Low Pass Filter |
RLC F-80-18-10-RF |
|
P |
|
800 MHz Low Pass Filter |
RLC F-30-800-RF |
|
P |
|
25 GHz Low Pass Filter
|
RLC F-80-25000-6-RF |
|
P |
|
1 GHz Notch Filter
|
Trilithic CFN-2-1000.1 |
|
P |
|
Adapters |
|||
|
Adapter, Type-N (f) to Type-N (f) |
1250-1472 |
|
A, P |
|
Adapter, Type-N (m) to Type-N (m) |
1250-1475 |
|
A, P, U |
|
Adapter, Type-N (m) to BNC (f) |
1250-1476 |
|
A, P |
|
Adapter, Type-N (m) to 3.5 mm (m) |
1250-1743 |
|
A, P, U |
|
Adapter, Type-N (m) to 3.5 mm (f)
|
1250-1744 |
|
A, P, U |
|
Adapter, Type-N (f) to 3.5 mm (f)
|
1250-1745 |
|
A, P, U |
|
Adapter, Type-N (f) to 3.5 mm (m) |
1250-1750 |
|
P |
|
Adapter, 3.5 mm (f) to 3.5mm (f)
|
83059B |
1250-1749 |
A, P, U |
|
Adapter, 3.5 mm (m) to 3.5 mm (m)
|
83059A |
1250-1748 |
P, A |
|
Adapter, 3.5 mm (m) to 3.5 mm (f) |
83059C |
|
P |
|
Adapter, 3.5
mm (f) to 2.4 mm (f)
|
11901B |
|
A, P, U |
|
Adapter, 3.5 mm (m) to 2.4 mm (f) |
11901D |
|
P, A, U |
|
Adapter, Type-N
(m) to 3.5 mm (m)
|
Maury CC-A-35N-MM |
|
A |
|
Adapter, Type-N
(m) to 2.4 mm (m)
|
11903A |
|
A, P |
|
Adapter, Type-N
(f) to 2.4 mm (f)
|
11903B |
|
A, P, U |
|
Adapter, Type-N
(m) to 2.4 mm (f)
|
11903D |
|
A, P, U |
|
Adapter, 2.4 mm (f) to 2.4 mm (f)
|
11900B |
|
A, P, U |
|
Adapter, BNC (m) to SMA (f) |
1250-1700 |
|
P |
|
BNC Tee (BNC f,m,f) |
1250-0781 |
|
P |
|
Adapter, BNC (f) to SMA (m) |
1250-1200 |
|
P |
|
Adapter, BNC (f) to Dual Banana |
1251-2277 |
|
P |
|
Adapter, 3.5 mm (f) to Type-N (m) |
08485-60005 |
|
A, P, U |
|
Adapter, 2.4 mm (f) to Type-N (m) |
08487-60001 |
|
A, P, U |
|
Type-N Tee |
1250-0559 |
|
P |
|
Optional Equipment |
|||
|
10 MHz Distribution Amplifier
|
Microsemi 5087B |
Microsemi 5087A |
P |
Keysight, Agilent, or Hewlett-Packard model numbers unless otherwise noted.
P = Performance Testing, T = Troubleshooting, A = Adjustments, U = Utilities
Microwave Signal Generator #1 should have one each of the following options:
Frequency Option:
567 (67 GHz) is recommended
High Power (E8257D only): Option 1EA (discontinued) or 1EU
E8267D
Two Phase Noise Test solutions are available. The Wenzel 500-13438D is an ultra low noise 1 GHz Oscillator. Although the EMI receiver does not require the performance of the Wenzel 500-13438D, other TME applications use the Wenzel solution, so the 500-13438D is an allowed instrument mapping. An alternate (and less expensive) solution is a PSG with Option UNR (or UNX) and a notch filter.
Wenzel
Associates Inc
2215 Kramer Ln
Austin, Texas 78758
(512) 835-2038
FAX (512) 719-4086
Both models of the Schwarzbeck pulse generator have fixed GPIB addresses which may require changing the GPIB address of conflicting equipment. Refer to the Connecting GPIB Test Instruments section of Getting Started.
N1914A power meters with serial number prefix prior to MY53040007 require Service Note N1914A-07 which fixes a power supply ground loop. The ground loop injects noise into the measurement circuits which can cause unstable measurements at low (–30 dBm) power levels.
The 8482A power sensor uses cal factors to compensate the power sensor for frequency response errors. Cal factors are stated in percentages. The 8482A factory cal factor uncertainty ranges from 2.2% to 3.1%. The cal factor uncertainty can be reduced to < 1.0% by using metrology grade calibration techniques. The power sensor cal factor uncertainty becomes one component of the Verification Test uncertainty analysis. Lower cal factor uncertainties will translate to wider test margins.
8485A power sensor frequency range specified in the data sheet starts from 50 MHz. To use the 8485A in Second Harmonic Intercept performance test, it needs to be calibrated from 10 MHz (add 10 MHz and 30 MHz frequency points).
When using the 10 MHz External Reference, be sure to update the Additional Properties in TME to the correct Frequency Accuracy in parts per million (ppm). For example, if overall accuracy is 9e-12, the equivalent is 9e-6 ppm. Refer to the Additional Properties section in the N7800A TME Help for instructions.
8491A/B Option H33 is a fixed attenuator which has been characterized to have a VSWR ≤ 1.05:1 at 50 MHz. A VSWR of 1.05:1 is recommended to test Input Attenuation Switching Uncertainty, Display Scale Fidelity, and Absolute Amplitude Accuracy performance tests. Any 8491A/B attenuator can be mapped into this device if the VSWR at 50 MHz has been characterized to be ≤ 1.05:1. When mapping the attenuator to indicate that it meets the required specification, Option H33 will need to be selected in the configure test station Administration screen.
The step attenuators should be permanently joined via the 11716A Interconnect Kit as shown in the diagram.
The step attenuator combination should have each attenuator setting characterized by a metrology lab at 50 MHz. This characterization can be ordered through Keysight Technologies as an Option H50 Calibration.
The following tables show which sections of the 10 dB and 1 dB step attenuators are utilized for each attenuator setting. The tables also list the Recommended Uncertainty for each attenuator setting. A larger number will result in larger overall test uncertainties which could affect the test pass/fail rate.
|
|
The interconnect cable should NEVER be disconnected once the loss characterization is performed. |
|
Nominal Attenuation |
Attenuator Section |
Recommended |
|||
|
#1 |
#2 |
#3 |
#4 |
||
|
0 |
Off |
Off |
Off |
Off |
0 (Reference) |
|
1 |
On |
Off |
Off |
Off |
< 0.005 |
|
2 |
Off |
On |
Off |
Off |
< 0.005 |
|
3 |
On |
On |
Off |
Off |
< 0.005 |
|
4 |
Off |
Off |
Ona |
Off |
< 0.005 |
|
5 |
On |
Off |
On |
Off |
< 0.005 |
|
6 |
Off |
On |
On |
Off |
< 0.005 |
|
7 |
On |
On |
On |
Off |
< 0.005 |
|
8 |
Off |
Off |
On |
On |
< 0.005 |
|
9 |
On |
Off |
On |
On |
< 0.005 |
|
Nominal Attenuation |
Attenuator Section |
Recommended |
|||
|
#1 |
#2 |
#3 |
#4 |
||
|
0 |
Off |
Off |
Off |
Off |
0 (Reference) |
|
10 |
On |
Off |
Off |
Off |
< 0.010 |
|
20 |
Off |
On |
Off |
Off |
< 0.015 |
|
30 |
On |
On |
Off |
Off |
< 0.020 |
|
40 |
Off |
Off |
Ona |
Off |
< 0.025 |
|
50 |
On |
Off |
On |
Off |
< 0.030 |
|
60 |
Off |
On |
On |
Off |
< 0.035 |
|
70 |
On |
On |
On |
Off |
< 0.040 |
|
|
The type of calibration kit (mechanical or ECal) depends on the test or utility. Refer to the table below and to the topic page for each test and utility.
|
Test / Utility |
Calibration kit |
|
Mechanical kit only |
|
|
Mechanical or ECal |
|
|
Network Analyzer Freq Sweep Calibration (Utility) |
ECal only |
Type-N and 3.5 mm mechanical calibration kit models are specific for the two VSWR performance tests. This is to ensure that the calibration kit has sufficient frequency range for the test. Use only the model numbers specified for each test.
Use the following guidelines to ensure power sensors used by the N7800A application receive the correct calibration service:
Order Option 1A7 when ordering new power sensors that will be used as working standards in N7800A TME calibrations.
When ordering periodic calibration for instruments used as lab standards in the N7800A software, we recommend using “Keysight Cal + Uncertainties + Guardbanding”. More information can be found at http://www.keysight.com/find/americas_cal.
The N7800A software incorporates the ISO GUM Uncertainty in point-to-point uncertainty calculations. The special “H-series” calibration options (shown on the Special Calibrations Matrix located at http://cal.software.keysight.com) provide lower measurement uncertainties through use of direct comparison to devices directly characterized by NPL or NIST (or another NMI). The overall resulting N7800A measurement uncertainties then reflects these lower device uncertainties. The equipment requirements of each N7800A calibration application are summarized in the Special Calibrations Matrix which can be found at http://cal.software.keysight.com.
Option H99 is a special option for the Roseville Service Center [only] which provides electronic calibration data available as a .csv file that can be imported into TME thus avoiding manual entry. Option H99 must be requested from the Roseville Service Center upon re-calibration only of any previously purchased power sensor and not for new purchases of power sensors. This option may be ordered in addition to any other required or requested Std Lab Calibration option. Option H99 is recommended but not required.
|
|
The following models are not supported by Option H99:
|
|
|
Failure to comply with the CalFactor(%) or Atten(dB) will result in test data being labeled Invalid in both the TME interface and in any report format produced from the data. |
| Device | Parameter Name and Description | Limits | A Failure Affects: |
|---|---|---|---|
|
Noise Source |
NoiseRatio(dB)
|
Must be > 0 and £ 30 |
All test runs |
|
Power Sensor |
CalFactor(%)
|
Must be ³
10% and £
150% at all points |
All test runs |
|
Uncertainty(%)
|
Must be > 0 and £ 10% at all points |
Test runs guard banded by measurement uncertainty only |
|
|
ReflectCoeff(Mag)
|
Must be >
0 and < 0.5 |
Test runs guard banded by measurement uncertainty only |
|
|
Power Sensor |
LowBandCalFactor(%)
|
Same tests as for CalFactor(%) on a one-range power sensor |
All test runs |
|
HighBandCalFactor(%)
|
Same tests as for LowBandCalFactor(%) |
All test runs |
|
|
LowBandUncertainty(%)
|
Same tests as for Uncertainty(%) on a one-range power sensor |
Test runs guard banded by measurement uncertainty only |
|
|
HighBandUncertainty(%)
|
Same tests as for LowBandUncertainty(%) |
Test runs guard banded by measurement uncertainty only |
|
|
ReflectCoeff(Mag)
|
Same tests as for ReflectCoeff(Mag) on a one-range power sensor |
Test runs guard banded by measurement uncertainty only |
|
|
Step Attenuator |
Atten(dB)
|
Must be within 1 dB of the nominal attenuation.
|
All test runs |
|
Uncert(dB)
|
Must be > 0 and £ 0.1 dB at all points except zero, zero step is the reference and must be zero |
Test runs guard banded by measurement uncertainty only |
|
|
ReflSize
|
Must be > 0 and < 0.5 at all points |
Test runs guard banded by measurement uncertainty only |