Troubleshooting Test Failures

If a test will not proceed, then suspect either the setup is incorrect, or the test equipment or DUT is faulty. Specifically you should:

If the test or adjustment can be completed as normal but fails, you should:

Performance Test Troubleshooting

The following performance tests have an associated troubleshooting procedure should problems be encountered. These troubleshooting procedures can be accessed with the following links.

  1. Internal Alignment Troubleshooting

  2. Frequency Reference Accuracy Troubleshooting

  3. Power Bandwidth Accuracy Troubleshooting

  4. Resolution Bandwidth Switching Uncertainty Troubleshooting

  5. MIL STD RBW Selectivity Troubleshooting

  6. Residual Responses Troubleshooting

  7. Displayed Average Noise Level Troubleshooting

  8. Effective DANL Troubleshooting

  9. Frequency Readout Accuracy Troubleshooting

  10. Frequency Span Accuracy Troubleshooting

  11. Count Accuracy Troubleshooting

  12. IF Frequency Response Troubleshooting

  13. RBW Selectivity CISPR Bands Troubleshooting

  14. Phase Noise Troubleshooting

  15. Absolute Amplitude Accuracy Troubleshooting

  16. Input Attenuation Switching Uncertainty Troubleshooting

  17. Display Scale Fidelity Troubleshooting

  18. Frequency Response Above 3.6 GHz (Preamp On) Troubleshooting

  19. EMI Receiver Mode Troubleshooting

  20. Spurious Responses Troubleshooting

  21. Frequency Response Above 3.6 GHz (Preamp Off) Troubleshooting

  22. Second Harmonic Distortion Troubleshooting

  23. Gain Compression Troubleshooting

  24. Third Order Intermodulation Distortion Troubleshooting

  25. Third Order Intermodulation Adjustment Troubleshooting

  26. Response to Pulses (Peak, Ave, RMS) Troubleshooting

  27. Variation with Pulse Repetition Freq (Ave, RMS) Troubleshooting

  28. Response to Intermittent Disturbances (Ave, RMS) Troubleshooting

  29. Radiated Band Sine Wave Accuracy Troubleshooting

  30. Frequency Response 50 MHz to 3.6 GHz Troubleshooting

  31. Frequency Response 9 kHz to 50 MHz Troubleshooting

  32. Conducted Band Sine Wave Accuracy Troubleshooting

  33. Frequency Response Below 300 kHz Troubleshooting

  34. Response to Pulses (Peak, Ave, RMS) Bands A/B/C/D Troubleshooting

  35. Q-P Detector Absolute Calibration Troubleshooting

  36. Q-P Detector Variation with Pulse Repetition Freq Troubleshooting

  37. Conducted Band VSWR Troubleshooting

  38. Radiated Band VSWR Troubleshooting