This test verifies the scale fidelity (linearity) of the EMI receiver at 50 MHz by comparing it to an external precision attenuator. As the external attenuation is increased in steps, the change in power level indicated by the DUT's display-marker is monitored. This test is performed in two parts so the step attenuator uncertainties are minimized.
The EMI receiver input attenuator is set to 10 dB in zero-span mode. The source is set to +10 dBm and the external composite attenuator is set to 19 dB. The resulting –25 dBm signal is measured by the DUT and recorded as the reference. The DUT input power is then varied between –11 dBm and –75 dBm (–21 dBm to –85 dBm at the mixer) by switching the external attenuator.
The EMI receiver input attenuator is set to 10 dB in zero-span mode. The source is set to +10 dBm and the external composite attenuator is set to 26 dB. The resulting –25 dBm signal is measured by the DUT and recorded as the reference. The input power is then varied between the –25 dBm and –6 dBm (–35 dBm to –16 dBm at the mixer) by switching the external attenuator.
|
|
|
Click here for troubleshooting.
|
Test Equipment |
Model Number1 |
|---|---|
|
Microwave Signal Generator #1 |
PSG Models |
|
Attenuator, 10 dB Fixed |
8491A Option 010, H33 |
|
Attenuator, 6 dB Fixed |
8491A Option 006, H33 |
|
Attenuator, 3 dB Fixed |
8491A Option 003, H33 |
|
Attenuator, 10 dB Step |
8496G Option 001, H50 |
|
Attenuator, 1 dB Step |
8494G Option 001, H50 |
|
Attenuator Driver |
11713B |
|
Attenuator Interconnect Kit |
11716A |
|
Cable, Type-N
|
11500C |
|
Cable, BNC |
8120-1840 |
|
Viking Cable (attenuator control) |
8120-2703 |
|
Adapter, 3.5 mm (f) to Type-N (f)
|
1250-1745 |
|
Adapter, 2.4 mm (f) to Type-N (f)
|
11903B |
|