FM distortion is defined as the square root of the ratio of the power contained in the harmonics of a demodulated FM waveform to the power of the fundamental component of the demodulated waveform.
This is essentially a Total Harmonic Distortion (THD) measurement and is made directly by the a spectrum analyzer with analog demodulation measurement application or an 8903B Audio Analyzer. The THD indicated includes the distortion added by the measuring receiver in demodulating the FM signal from the DUT.
This test is currently performed in only one frequency band. Due to the signal generator’s design, this band is also representative of the signal generator’s full frequency range.
This test supports two equipment setups using either a spectrum analyzer or a measuring receiver. The spectrum analyzer is the preferred solution.
A spectrum analyzer with analog demodulation measurement application is used to demodulate the signal and measure the deviation.
|
Test Equipment |
Recommended Models |
Alternative Models |
|
Spectrum Analyzer |
N9030B Opt 5xx1, N9063EM0E Analog Demodulation Measurement application |
N9030A2 Opt 5xx1, N9063EM0E Analog Demodulation Measurement application E444xA3 Opt 233 Measuring Receiver Personality |
|
Alternatively, an 8902A measuring receiver is used to demodulate the signal and measure the deviation.
|
Test Equipment |
Recommended Models |
|
Measuring Receiver |
8902A |
|
Audio Analyzer |
8903B |
|
|
|
Connect all test equipment as shown.
Connect GPIB cables to all GPIB-controlled test equipment.
While performing this performance test, follow all instructions on the controller display.
Setup for Internal FM Distortion
Setup for Measuring Receiver Calibration
Setup for Internal FM Distortion
If this performance test fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the Performance Test.
If this test fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.