Internal FM Frequency Response verifies that a selected FM deviation remains constant within ± 1 dB as the FM rate is varied from 80 Hz to 100 kHz and the DUT CW frequency is varied from 500 MHz to 1.0 GHz. If the DUT meets the frequency response specification in this CW frequency range, frequency response in all other frequency ranges will be assured.
FM deviation is set to 100 kHz at an FM rate of 1 kHz. The actual deviation is measured with a measuring receiver and stored as the reference deviation. While the deviation setting remains at 100 kHz, actual deviation is measured for FM rates between 80 Hz and 100 kHz. If the measured deviation at any test rate is more than 1 dB different from the reference deviation at 1 kHz, the test fails.
This test supports two equipment setups using either a spectrum analyzer or a measuring receiver. The spectrum analyzer is the preferred solution.
A spectrum analyzer with analog demodulation measurement application is used to demodulate the signal and measure the deviation.
|
Test Equipment |
Recommended Models |
Alternative Models |
|
Spectrum Analyzer |
N9030B Opt 5xx1, N9063EM0E Analog Demodulation Measurement application |
N9030A2 Opt 5xx1, N9063EM0E Analog Demodulation Measurement application E444xA3 Opt 233 Measuring Receiver Personality |
|
Alternatively, an 8902A measuring receiver is used to demodulate the signal and measure the deviation.
|
Test Equipment |
Recommended Models |
|
Measuring Receiver |
8902A |
|
|
|
Connect all test equipment as shown.
Connect GPIB cables to all GPIB-controlled test equipment.
While performing this performance test, follow all instructions on the controller display.
Internal FM Frequency Response Test Setup
Setup for Measuring Receiver Calibration
Setup for FM Frequency Response Test
If this performance test fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the Performance Test.
If this test fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.