This test compares the selected ΦM (phase-modulation) deviation to the measured ΦM deviation. This test is currently performed in only one frequency band. Due to the signal generator’s design, this band is also representative of the signal generator’s full frequency range.
A measuring receiver is used to demodulate the ΦM signal and indicate the recovered phase deviation. In order to increase the accuracy of the measurement (that is, lower the uncertainty), the ΦM signal is demodulated by the FM demodulator of the measuring receiver. The measured FM deviation is then divided by the FM/PM rate to obtain the PM deviation.
This test supports two equipment setups using either a spectrum analyzer or a measuring receiver. The spectrum analyzer is the preferred solution.
A spectrum analyzer with analog demodulation measurement application is used to demodulate the signal and measure the deviation.
|
Test Equipment |
Recommended Models |
Alternative Models |
|
Spectrum Analyzer |
N9030B Opt 5xx1, N9063EM0E Analog Demodulation Measurement application |
N9030A2 Opt 5xx1, N9063EM0E Analog Demodulation Measurement application E444xA3 Opt 233 Measuring Receiver Personality |
|
Alternatively, an 8902A measuring receiver is used to demodulate the signal and measure the deviation.
|
Test Equipment |
Recommended Models |
|
Measuring Receiver |
8902A |
|
|
|
Connect all test equipment as shown.
Connect GPIB cables to all GPIB-controlled test equipment.
While performing this performance test, follow all instructions on the controller display.
Setup for Internal Phase Modulation Deviation Accuracy
Setup for Measuring Receiver Calibration
Setup for Internal Phase Modulation Deviation Accuracy
If this performance test fails, perform the following steps in order:
Check the equipment setup (see above). If the setup is incorrect, make the necessary corrections and rerun the Performance Test.
If this test fails with the equipment set up properly, refer to the troubleshooting section of the signal generator's service guide. If you do not have a printed copy of the service guide (Option OBW), one is available either on the CD-ROM that came with your signal generator shipment or on the Keysight Website.
If you cannot correct the problem using the troubleshooting procedures in the Service Guide, obtain service from Keysight Technologies. Refer to Contacting Keysight Technologies.