|
|
|
There are two solutions offered in the Normal Variant test plan for the Dynamic Accuracy Performance Test depending on model and option combination or serial number prefix break. Each solution uses a different dynamic accuracy test set. Use the Decision Tree below to determine which solution is appropriate for your model.
|
Preferred Solution |
Uses the U3020BD01 or U3020AD01 test set |
|
Alternate Solution |
Uses the Z5623A Opt. H01 test set |
|
Dual Solution |
Some models will use a dual solution meaning that either solution can be used depending on which dynamic accuracy test set is mapped in TME. If both test sets are mapped, TME will recommend the Preferred Solution. |
Some PNA-X models (depending on serial number) are assigned Option <NDA> in TME to facilitate testing. Refer to the table below to determine if your model is assigned Option <NDA>. Models with this option will always use the Preferred Solution.
|
Model Number |
Serial Number Prefix |
Model Number |
Serial Number Prefix |
|
|
Models with serial prefix greater than or equal to these will be assigned Option <NDA> in TME. |
Models with serial prefix greater than or equal to these will be assigned Option <NDA> in TME. |
|||
|
N5241A |
MY5241 |
N5241AS |
MY5246 |
|
|
N5242A |
MY5242 |
N5242AS |
MY5247 |
|
|
N5244A |
MY5244 |
N5244AS |
MY5249 |
|
|
N5245A |
MY5245 |
N5245AS |
MY5250 |
|
Use the interactive Decision Tree diagram below to determine which solution applies to your model number. (Hover the mouse over text for tips and links.)
|
|
This Decision Tree applies to Normal Variant test plans only. For models using the Factory Recommended Variant test plan, see Dynamic Accuracy — Factory Recommended Variant. |