N5241A/AS/B/BC, N5242A/AS/B, N5242AH85, N5249A/AS/B
N5221A/AS/B, N5222A/AS/B
N5231A/AS/B, N5232A/AS/B, N5239A/AS/B
N5230A/C with option 12x, 14x, 22x, 24x, or 02x
N5244A/AS/B, N5245A/AS/B/BC
N5224A/AS/B, N5225A/AS/B
N5234A/AS/B, N5235A/AS/B
N5230A/C with option 42x or 52x
N5247A/AS/B/BC, N5227A/AS/B
N5290A, N5291A
|
|
This test is extremely sensitive. To minimize the chance of test failure, it is important to follow proper testing procedures:
|
This topic shows the required equipment and connection setups for PNA models running the Factory Recommended Variant test plan. For more information about test plan variants, refer to the Test Plan Variants topic.
For models with Low Frequency Extension option (LFE), there is an additional test procedure. Refer to the Dynamic Accuracy at Low Frequency topic page.
For PNA mmWave Systems N5290A and N5291A.
|
1 mm Connector Models |
|
|
Test Equipment1 |
Recommended Model |
|
Function generator |
33622A |
|
Power splitter |
11667B |
|
Fixed attenuator, 10 dB |
8493C Option 010 |
|
For all other PNA models.
|
Test Equipment1 |
Recommended Model |
Alternate Model |
|
Power meter |
N1914B |
N1914A |
|
PowerSensor 1, for 3.5 mm models |
U8485A2 Opt. 200 |
U8485A2 |
|
PowerSensor 1, for 2.4 mm models |
U8488A2 |
U8487A2 |
|
PowerSensor 1, for 1.85 mm models |
U8488A2 |
N8488A3 |
|
Dynamic Accuracy test set4 |
U3020BD01 |
U3020AD01 |
|
Signal Generator |
E8257D |
N5183B E8257C E8247C (not allowed for N5241x and N5242x PNA-X) |
|
Load, 3.5 mm 50 W |
909D |
902C |
|
|
|
Due to the complexity of the PNA family of analyzers, the following notes apply to illustrations in the PNA Help:
|
PNA models running the Factory Recommend Variant will use flexible power sensor channel assignment that will identify the channel that a power sensor is connected to using the ability of "smart" sensors such as the N848xA and U848xA series to report their full model and serial number. Therefore it is important to keep the power sensor on the channel where it was calibrated throughout the test procedures.
For more information about test plan variants, refer to the Test Plan Variants topic.
For default front and rear cabling between the PNA and the test set, refer to Step 2: Prepare the PNA for Testing of the Getting Started Guide.
|
|
For the two cables between the power splitter and attenuators, choose short but flexible cables. For best results, the cable between the attenuator on channel 1 of the function generator and power splitter should be of longer length than the cable from the attenuator on channel 2. |