This test verifies the frequency accuracy and range of the PNA's source output, and verifies the Test Port Output – CW Accuracy specification.
For single source PNAs, this test is only performed on Port 1, and the specification only applies to this port. For dual source PNAs, Port 3 is also tested. The process is the same as for Port 1.
Power levels:
Microwave PNA = -17 dBm or higher
For troubleshooting help, see Frequency Accuracy Troubleshooting.
Options in angle brackets such as <SYN> are assigned by TME to facilitate testing and do not reflect product options. PNA models with a high-accuracy synthesizer have a different frequency accuracy specification than models without the high-accuracy synthesizer. (Refer to the product datasheet for information regarding the product specifications.) These models will be assigned option <SYN> by TME to support testing required for the different specification. Note that PNA models assigned option <SYN> can only run the Recommended Variant.
To determine if the UUT has this high-accuracy synthesizer and will therefore be assigned option <SYN> in TME, open the
About window on the PNA. If the Synthesizer Revision is 7.0 or greater, the UUT will have the high-accuracy synthesizer. These models will also run the Initial Frequency Accuracy test to verify this test.
Can only use frequency counter models:
53132A with Options 012 and 124
The frequency accuracy of an external house standard must be 1.e-8 or less.
Below is the required test equipment for this test. Select the link that applies to your model.
Table A: PNA microwave models:
N5230A/C Opt. 02x, 12x, 14x, 22x, 24x
N5241A/AS/B/BC, N5242A/AS/B, N5242AH85, N5249A/AS/B
N5221A/AS/B, N5222A/AS/B
N5231A/AS/B, N5232A/AS/B, N5239A/AS/B
Table B: PNA microwave models:
N5230A/C Opt. 42x, 52x
N5244A/AS/B, N5245A/AS/B/BC, N5247A/AS/B/BC
N5224A/AS/B, N5225A/AS/B, N5227A/AS/B
N5234A/AS/B, N5235A/AS/B
Table C: PNA mm-Wave system models:
N5290A, N5291A
|
PNA Microwave Analyzers: |
||
|
N5230A/C Opt. 02x, 12x, 14x, 22x, 24x |
||
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Frequency counter |
53230A1 Opt. 010 and 115 |
53132A1 Opt. [010 or 012] and 124 53131A Opt. 010 and 124 53181A Opt. 010 and 124 53150A/51A/52A2 Opt. 001 |
|
Frequency Reference 3 |
House standard3, 4 |
Frequency counter's internal frequency reference |
|
Adapter Type-N (m) to 3.5 mm (m) |
1250-1743 |
equivalent |
|
Adapter Type-N (f) to BNC (m) |
1250-1477 |
equivalent |
|
Adapter 3.5 mm (m) to 3.5 mm (m) |
1250-1478 |
83059A |
|
Adapter SMA (f) to BNC (m) |
1250-2015 |
equivalent |
|
Cable RF 3.5 mm (f) to 3.5 mm (f) |
85131-60013 |
85131-60010 |
|
|
PNA Microwave Analyzers: |
||
|
N5230A/C Opt. 42x, 52x |
||
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Frequency counter1 |
53230A Opt. 010 and 115 |
53132A Opt. [010 or 012] and 124 53131A Opt. 010 and 124 53181A Opt. 010 and 124 53150A/51A/52A2 Opt. 001 |
|
Frequency Reference 3 |
House standard3, 4 |
Frequency counter's internal frequency reference |
|
Adapter Type-N (m) to 2.4 mm (m) |
11903A |
equivalent |
|
Adapter Type-N (f) to BNC (m) |
1250-1477 |
equivalent |
|
Adapter 3.5 mm (m) to 2.4 mm (m) |
11901A |
equvalent |
|
Adapter SMA (f) to BNC (m) |
1250-2015 |
equivalent |
|
Cable RF 2.4 mm (f) to 2.4 mm (f) or Cable RF 1.85 mm (f) to 1.85 mm (f) |
85133-60016 or N4697-60010 |
85133-60002
|
|
|
PNA mm-Wave systems: |
||
|
N5290A, N5291A |
||
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Frequency counter1 |
53230A Opt. 010 and 115 |
53132A Opt. [010 or 012] and 124 53131A Opt. 010 and 124 53181A Opt 010 and 124 |
|
Frequency Reference 2 |
House standard2, 3 |
Frequency counter's internal frequency reference |
|
|
|
Due to the complexity of the PNA family of analyzers, the following notes apply to illustrations in the PNA Help:
|
For default front and rear cabling between the PNA and the test set, refer to Step 2: Prepare the PNA for Testing of the Getting Started Guide.
|
|
The section below refers to FreqReference2 and FreqCounter2 Internal Ref which are present if the Factory Recommended test plan variant is selected. If the Normal test plan variant is selected, then the user will see FreqReference1 and FreqCounter1 Internal Ref. For the purpose of the explanation below, these are interchangeable. |
The equipment list for this test includes a FreqReference2. The model for this equipment type may be 10 MHz External Reference (house standard) or FreqCounter2 Internal Ref which uses the internal frequency reference of the frequency counter with applicable options. When 10 MHz External Reference is specified, an external 10 MHz reference is required to be connected to the counter.
The external 10 MHz "house standard" is recommended due to larger MU caused by using the internal frequency reference of the frequency counter.
The calibration date, etc, for FreqCounter2 Internal Ref should match the frequency counter. The calibration information for 10 MHz External Reference will depend on the source used for the 10 MHz.
When 10 MHz External Reference is specified, the user must provide a value for frequency accuracy. Frequency Accuracy represents the worst case accuracy of the reference (maximum deviation from exactly 10 MHz) any time during the calibration period of the reference. The value is expressed in ppm and is entered via the Additional Properties key.
As an example, if the accuracy of an external frequency reference is +/- 1.0 Hz, then the accuracy is 1.0e-7. The value in ppm would be entered as 0.10.
|
|
For PNA models assigned option <SYN>, the frequency accuracy of an external house standard must be 1.e-8 or less. See Option <SYN> above for more information. |
The table below shows some examples of estimated frequency accuracy values if a separate counter is used as the 10 MHz External Reference instead of a house standard, based on 1-year stability specifications.
Note that these are not final uncertainty numbers for frequency accuracy tests. Furthermore, any reference value above 0.2 ppm is likely to produce unsatisfactory measurement uncertainties.
|
Model |
Option |
Value |
|
53131A/32A |
no options |
9.93 ppm |
|
001 |
2.78 ppm |
|
|
010 |
0.22 ppm |
|
|
53132A |
012 |
0.062 ppm |
|
53181A |
no options |
9.93 ppm |
|
001 |
2.78 ppm |
|
|
010 |
0.22 ppm |
|
|
53151A |
no options |
2.14 ppm |
|
001 |
0.22 ppm |
|
|
53230A |
no option |
2.26 ppm |
|
010 |
0.082 ppm |
|