Initial Frequency Accuracy

The Frequency Accuracy Performance Test must be run within seven days prior to running this test.

This test applies to the following models with option <SYN>:

This functional test will verify that the performance reported by the Frequency Accuracy Performance Test meets the new Initial Frequency Accuracy specification. PNA models with a high-accuracy synthesizer have a different frequency accuracy specification than models without the high-accuracy synthesizer. This test is needed to verify the new specification for those models. To facilitate testing, TME will assign option <SYN> to PNA models with this high-accuracy synthesizer. See Option <SYN> below for more information and for equipment requirements. This test will only appear if the DUT is assigned option <SYN>.

This test will use data collected from the Frequency Accuracy Performance Test. Note that the data collected must be from within the previous seven days. TME will request the operator to re-run the Frequency Accuracy Performance Test if it's been longer than the seven days.

If the results from the Frequency Accuracy Performance Test are insufficient for the Initial Frequency Accuracy test, then the operator will be asked to run the 10 MHz Frequency Reference Adjustment on the PNA. To run the adjustment, on the PNA press UTILITY > System > Service > Adjustment Routines > 10 MHz Freq Adjustment. After running the adjustment, re-run the Initial Frequency Accuracy test.

Option <SYN>

Options in angle brackets such as <SYN> are assigned by TME to facilitate testing and do not reflect product options. PNA models with a high-accuracy synthesizer have a different frequency accuracy specification than models without the high-accuracy synthesizer. (Refer to the product datasheet for information regarding the product specifications.) These models will be assigned option <SYN> by TME to support testing required for the different specification.

To determine if the UUT has this high-accuracy synthesizer and will therefore be assigned option <SYN> in TME, open the ClosedAbout window on the PNA. If the Synthesizer Version is 7.0 or greater, the UUT will have the high-accuracy synthesizer.

Equipment requirements for models assigned option <SYN>

Required Test Equipment

Test Equipment

Recommended Model

Alternate Model

Frequency counter

53230A Opt. 010 and 115

53132A Opt. [010 or 012]1 and 124

Frequency Reference 2

House standard3

Frequency counter's internal frequency reference

Adapter Type-N (m) to 3.5 mm (m)

1250-1743

equivalent

Adapter Type-N (f) to BNC (m)

1250-1477

equivalent

Adapter SMA (f) to BNC (m)

1250-2015

equivalent

Cable RF 3.5 mm (f) to 3.5 mm (f)

85131-60013
(more flexible)

85131-60010
(less flexible)

Cable RF 2.4 mm (f) to 2.4 mm (f)

or

Cable RF 1.85 mm (f) to 1.85 mm (f)

85133-60016

or

N4697-60010

85133-60002
(less flexible)

 

BNC cable

any

any

  1. For the 53132A:

    • Option 012 (ultra-high stability timebase) is required when using an internal frequency reference.
    • Option 010 (high stability timebase) is allowed when using an external frequency reference providing it has a frequency accuracy of 1.e-8 or less.

  2. The frequency reference may come from an external 10 MHz "house standard" (which is recommended), or it may come from using the internal frequency reference time-base of the frequency counter used for the frequency measurement.

    The 10 MHz "house standard" is recommended due to larger MU caused by using the internal frequency reference of the frequency counter.

    See Frequency Reference Explanation below.

  3. The frequency accuracy of a house standard must be 1.e-8 or less. See Option <SYN> for more information.

Connection Setups

Due to the complexity of the PNA family of analyzers, the following notes apply to illustrations in the PNA Help:

  • Only a single representative PNA model will be shown. Therefore, port locations may differ in older PNA models than what is shown in the illustration. Refer to the port labels on the UUT.
  • Some illustrations may differ than those in TME.
  • If the test procedure applies to multiple ports, illustrations may show the setup on only one test port.
  • Setups for some option configurations may not appear in the Help.

 

Frequency Reference Explanation

The equipment list for this test includes a FreqReference2. The model for this equipment type may be 10 MHz External Reference (house standard) or FreqCounter2 Internal Ref which uses the internal frequency reference of the frequency counter with applicable options. When 10 MHz External Reference is specified, an external 10 MHz reference is required to be connected to the counter.

The external 10 MHz "house standard" is recommended due to larger MU caused by using the internal frequency reference of the frequency counter.

The calibration date, etc, for FreqCounter2 Internal Ref should match the frequency counter. The calibration information for 10 MHz External Reference will depend on the source used for the 10 MHz.

When 10 MHz External Reference is specified, the user must provide a value for frequency accuracy. Frequency Accuracy represents the worst case accuracy of the reference (maximum deviation from exactly 10 MHz) any time during the calibration period of the reference. The value is expressed in ppm and is entered via the Additional Properties key.

As an example, if the accuracy of an external frequency reference is +/- 1.0 Hz, then the accuracy is 1.0e-7. The value in ppm would be entered as 0.10.

For PNA models assigned option <SYN>, the frequency accuracy of an external house standard must be 1.e-8 or less. See Option <SYN> above for more information.

Frequency Accuracy Values

The table below shows some examples of estimated frequency accuracy values if a separate counter is used as the 10 MHz External Reference instead of a house standard, based on 1-year stability specifications.

Note that these are not final uncertainty numbers for frequency accuracy tests. Furthermore, any reference value above 0.2 ppm is likely to produce unsatisfactory measurement uncertainties.

Frequency Accuracy Value Examples

Model

Option

Value

53132A

012

0.062 ppm

53230A

no option

2.26 ppm

010

0.082 ppm