N5244AS, N5245AS with Option H29
This test is to measure the worst case compression of the RF components of the noise receiver. The noise receiver compression is, as with all compression, a measurement of the non-linearity of the noise receiver at high input powers. This test has been defined to measure the compression, or linearity, of the noise receiver at a specified input-power level relative to a lower power level that is within the receiver’s linear range. For this test, compression is defined as the difference between the change in power input to the receiver and the change in power measured by the receiver.
The PNA source will provide the power at the receiver. A pad can be used to improve the match of the source over power. This may be required because the noise receiver is sensitive to match changes which could happen with input power changes. The source output power is measured and adjusted as necessary to ensure that the appropriate test power level is injected into the port. The source is then connected to the noise receiver port.
At each frequency the source is set to output the required power, and a measurement is taken with the noise receiver. The power delivered to the port is measured with the port receiver (can be frequency swept measurement). The source power is next offset by the specified power step (delta power) and a measurement is again taken with each receiver.
For troubleshooting help, see Noise Receiver Compression Troubleshooting.
Below is the required test equipment separated by the DUT connector type. Select the link that applies to the connector type for your PNA model.
N5241A/AS/B/BC, N5242A/AS/B, N5242AH85, N5249A/AS/B
|
3.5 mm Connector Models |
||
|
Test Equipment1 |
Recommended Model |
Alternate Model |
|
Power meter |
N1914B |
N1914A |
|
PowerSensor 1 |
U8485A2 Option 200 |
U8485A2 |
|
10 dB Fixed Attenuator, 3.5 mm |
8493C Opt. 010 |
none |
|
|
3.5 mm Connector Models |
||
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Power Meter |
N1914A |
E4419A/B |
|
PowerSensor HighFreq 1 |
N8485A |
N8485A CFT |
|
10 dB Fixed Attenuator |
8493C Opt. 010 |
none |
|
Adapter, 3.5 mm (m) to Type-N (f) |
1250-1750 |
none |
|
RF cable, 3.5 mm (f) to 3.5 mm (f) |
85131-60013 |
85131-60010 |
N5244A/AS/B, N5245A/AS/B/BC
|
|
PNA models N5244AS and N5245AS with option H29 can only use the Normal Variant. |
|
2.4 mm Connector Models |
||
|
Test Equipment1 |
Recommended Model |
Alternate Model |
|
Power meter |
N1914B |
N1914A |
|
PowerSensor 1 |
U8488A2 |
U8487A2 |
|
10 dB Fixed Attenuator, 2.4 mm |
8490D Opt. 010 |
none |
|
|
2.4 mm Connector Models |
||
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Power Meter |
N1914A |
E4419A/B |
|
PowerSensor HighFreq 1 |
N8487A |
N8487A CFT |
|
10 dB Fixed Attenuator |
8490D Opt. 010 |
none |
|
Adapter, 2.4 mm (m) to Type-N (f) |
11903C |
equivalent |
|
RF Cable 2.4 mm (f) to 2.4 mm (f) |
85133-60016 |
85133-60002 |
N5247A/AS/B/BC
|
1.85 mm Connector Models |
||
|
Test Equipment1 |
Recommended Model |
Alternate Model |
|
Power meter |
N1914B |
N1914A |
|
PowerSensor 1 |
U8488A2 |
N8488A3 |
|
10 dB Fixed Attenuator, 1.85 mm |
8490G Opt. 010 |
Anritsu 41V-10 |
|
|
For 1.85 mm Connector Models |
||
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Power Meter |
N1914A |
E4419A/B |
|
PowerSensor HighFreq 1 |
N8487A |
N8487A CFT |
|
10 dB Fixed Attenuator |
8490G Opt. 010 |
Anritsu 41V-10 |
|
Adapter, 2.4 mm F to Type-N (m) |
11903D |
equivalent |
|
RF cable, 1.85 mm (f) to 1.85 mm (f) |
8121-2921 |
N4697-60100 |
|
|
Due to the complexity of the PNA family of analyzers, the following notes apply to illustrations in the PNA Help:
|
PNA models running the Factory Recommend Variant will use flexible power sensor channel assignment that will identify the channel that a power sensor is connected to using the ability of "smart" sensors such as the N848xA and U848xA series to report their full model and serial number. Therefore it is important to keep the power sensor on the channel where it was calibrated throughout the test procedures.
For more information about test plan variants, refer to the Test Plan Variants topic.