There are now two test plan variants offered in the N7840A PNA Calibration Application:
Normal Variant
Factory Recommended Variant
The Factory Recommended Variant is the preferred variant because it optimizes test times with reduced connections and supports updated test equipment. Legacy ETE is supported in the Normal Variant. Some PNA models can only use one of the variants as explained in this topic. For models that can use either variant, test results will be identical in either variant.
Note the following for the Factory Recommended Variant test plan:
The following PNA models are not supported:
N5247AS with Option H29
N5230A/C models using the Factory Recommended Variant require firmware version ≥ A.09.00.
The following PNA models can only use the Factory Recommended Variant:
N522xB and N524xB, N5241BC, N5245BC, and N5247BC assigned by TME with option <SYN>. For an explanation of option <SYN>, see Option <SYN> in the Frequency Accuracy Performance Test topic.
Includes all tests from the Normal Variant plus two new tests for LFE options:
The following tests have combined the below 50 GHz and above 50 GHz tests:
Legacy test equipment such as 84xxA power sensors and Z5623A test sets are not supported in the Factory Recommended Variant.
Calibration Coefficients Performance Test and Noise State Calibration Coefficients Performance Test in the Factory Recommended Variant have been enhanced to use an unknown thru functionality that reduces the number of connections required in the test.
For some tests, certain test equipment such as cables and adapters are no longer required to be mapped due to improved test processes. This will save the operator time when setting up test station.
The Factory Recommended Variant supports USB U-series power sensors and flexible power sensor channel assignment which allows for connections on all four channels on the power meter:
USB channels C and D for U-series USB sensors
This flexibility significantly reduces the number of power sensor connections which in turn reduces overall test times. In some cases, the number of connections are reduced by more than half as shown in the examples below:
|
Example DUT |
Normal Variant |
Factory Recommended Variant |
|
2.4 mm 4-port |
32 power sensor connections |
16 power sensor connections |
|
1.85 mm 3-port |
48 power sensor connections |
20 power sensor connections |
The Normal Variant allows the operator to use legacy test equipment such as 84xxA power sensors and Z5623A test sets. The following PNA models can only use the Normal Variant test plan:
N5247AS with Option H29