N5244AS, N5245AS with Option H29
|
|
Before running this test, certain settings must be set in TME and the PNA. For TME:Be sure that For the PNA:Select Enable Remote Drive Access. Go to Utilities > System > System Setup > Remote Interface
|
This test checks the match term at the port of the noise hardware of a vector network analyzer in the noise measurement state.
The filtered source is turned ON and the signal level is measured at the splitter output port with a power meter. The filtered source amplitude is measured on the analyzer. The unfiltered source is turned ON and its amplitude is measured on the analyzer using the analyzer’s delta-marker feature. The amplitude of the distortion product is then measured relative to the unfiltered source amplitude.
For troubleshooting help, see Noise Receiver Match Troubleshooting.
Below is the required test equipment separated by the DUT connector type. Select the link that applies to the connector type for your PNA model.
|
|
|
N5241A/AS/B/BC, N5242A/AS/B, N5242AH85, N5249A/AS/B
|
Calibration Kits for |
|||
|
|
ECal Modules |
Mechanical3 |
|
|
Test Plan Variants |
N4691D2 Options 0DC, M0F |
N4691-60004 N4691-60008 |
85052B 85052D |
|
Factory Recommended |
X |
X |
X |
|
Normal |
|
X |
X |
|
N5244A/AS/B, N5245A/AS/B/BC
|
Calibration Kits for |
|||
|
|
ECal Modules |
Mechanical3 |
|
|
Test Plan Variants |
N4693D2 Options 0DC, M0F N4693-61001 |
N4693-60001 |
85056A |
|
Factory Recommended |
X |
X |
X |
|
Normal |
|
X |
X |
|
N5247A/AS/B/BC
|
Calibration Kits for |
|||
|
|
ECal Modules |
Mechanical3 |
|
|
Test Plan Variants |
N4694D2 Options 0DC, M0F |
N4694-60001 |
85058B |
|
Factory Recommended |
X |
X |
X |
|
Normal |
|
X |
X |
|
|
|
Due to the complexity of the PNA family of analyzers, the following notes apply to illustrations in the PNA Help:
|