|
|
This test process will reset the cal kit definitions to factory defaults; therefore custom cal kit definitions will be lost. |
N5244AS, N5245AS with Option H29
This test is the same procedure as the standard Calibration Coefficients performance test with the following exceptions:
For standard Calibration Coefficients, the port 1 noise tuner switch is set to external, and an unknown thru calibration procedure is used.
For Noise State Calibration Coefficients, the port 1 noise tuner is set to internal, and the test uses a multiple flush-thru calibration approach.
Be sure that
Pause on test point fail is not selected for this test.
For troubleshooting help, see Troubleshooting.
Below is the required test equipment separated by the DUT connector type. Select the link that applies to the connector type for your PNA model.
|
|
|
N5241A/AS/B/BC, N5242A/AS/B, N5242AH85, N5249A/AS/B
|
Calibration Kits for |
|||
|
|
ECal Modules |
Mechanical3 |
|
|
Test Plan Variants |
N4691D2 Options 0DC, M0F |
N4691-60004 N4691-60008 |
85052B 85052D |
|
Factory Recommended |
X |
X |
X |
|
Normal |
|
X |
X |
|
N5244A/AS/B, N5245A/AS/B/BC
|
Calibration Kits for |
|||
|
|
ECal Modules |
Mechanical3 |
|
|
Test Plan Variants |
N4693D2 Options 0DC, M0F N4693-61001 |
N4693-60001 |
85056A |
|
Factory Recommended |
X |
X |
X |
|
Normal |
|
X |
X |
|
N5247A/AS/B/BC
|
Calibration Kits for |
|||
|
|
ECal Modules |
Mechanical3 |
|
|
Test Plan Variants |
N4694D2 Options 0DC, M0F |
N4694-60001 |
85058B |
|
Factory Recommended |
X |
X |
X |
|
Normal |
|
X |
X |
|
|
|
Due to the complexity of the PNA family of analyzers, the following notes apply to illustrations in the PNA Help:
|