|
|
|
This topic shows the required equipment and connection setups for PNA models running the Normal Variant test plan. For more information about test plan variants, refer to the Test Plan Variants topic.
For test description, go to the topic's Overview page.
Below is the required test equipment separated by the DUT connector type. Select the link that applies to the connector type for your PNA model.
N5241A/AS/B/BC, N5242A/AS/B, N5242AH85, N5249A/AS/B
N5221A/AS/B, N5222A/AS/B
N5231A/AS/B, N5232A/AS/B, N5239A/AS/B
N5230A/C with option 12x, 14x, 22x, 24x, or 02x
|
3.5 mm Connector Models |
||
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Power meter |
N1914A |
E4419A/B |
|
PowerSensor LowFreq 1 |
N8482A |
N8482A-CFT |
|
PowerSensor HighFreq 1 |
N8485A |
N8485A-CFT |
|
Gain Compression Test Set
|
Z5623A Opt. K01 |
none |
|
Gain Compression Test Set |
U3070AK01 |
Z5623A Opt. K01 |
|
10 dB fixed attenuator
|
8493C Opt. 010 |
none |
|
20 dB fixed attenuator, 3.5 mm For these models:
|
8493C Opt. 020 |
|
|
Power sensor cable
|
11730A |
equivalent |
|
Cable RF 3.5 mm (f) to 3.5 mm (f)
|
85131-60013 |
85131-60010 |
|
Adapter 3.5 mm (m) to 2.4 mm (f) |
11901D |
equivalent |
|
Adapter 3.5 mm (m) to 2.4 mm (f)
|
85130-60010 |
none |
|
Adapter 3.5 mm (m) to Type-N (f) |
1250-1750 |
equivalent |
|
Adapter 3.5 mm (f) to Type-N (m)
|
1250-1744 |
08485-60005 |
N5230A Opt. 42x, 52x
N5230C Opt. 42x, 52x
N5244A/AS/B, N5245A/AS/B/BC
N5224A/AS/B, N5225A/AS/B
N5234A/AS/B, N5235A/AS/B
|
2.4 mm Connector Models |
||
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Power meter |
N1914A |
E4419A/B |
|
PowerSensor LowFreq 1 |
N8482A |
N8482A-CFT |
|
PowerSensor HighFreq 1 |
N8487A |
N8487A-CFT |
|
Gain Compression Test Set
|
Z5623A Opt. K01 |
none |
|
Gain Compression Test Set
|
U3070AK01 |
Z5623A Opt. K01 |
|
20 dB fixed attenuator, 2.4 mm
|
8490D Opt. 020 |
|
|
Cable RF 2.4 mm (f) to 2.4 mm (f)
|
85133-60016 |
85133-60002 |
|
Cable 2.4 mm (f) to 2.4 mm (m)
|
8121-2065 |
none |
|
Power sensor cable
|
11730A |
equivalent |
|
Adapter 2.4 mm (m) to Type-N (f) |
11903C |
equivalent |
|
Adapter 2.4 mm (f) to Type-N (m)
|
11903D |
08487-60001 |
N5247A/AS/B/BC. N5227A/AS/B
|
1.85 mm Connector Models |
||
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Power meter |
N1914A |
E4419A/B |
|
PowerSensor LowFreq 1 |
N8482A |
N8482A-CFT |
|
PowerSensor HighFreq 1 |
N8487A |
N8487A-CFT |
|
PowerSensor UltraHighFreq 1 |
N8488A |
V8486A with the V281A waveguide adapter1 |
|
Gain Compression Test Set
|
U3070BK013 |
U3070AK013 |
|
20 dB fixed attenuator, 1.85 mm
|
8490G Opt. 020 |
Anritsu 41V-20 |
|
Cable 1.85 mm (f) to 1.85 mm (m)
|
8121-2064 |
none |
|
Cable 2.4 mm (f) to 2.4 mm (m)
|
8121-2065 |
none |
|
Power sensor cable
|
11730A |
equivalent |
|
Adapter 1.85 mm (m) to 1.85 mm (m)
|
85058-60113 |
none |
|
Adapter 2.4 mm (f) to Type-N (f) |
11903B |
equivalent |
|
Adapter 2.4 mm (f) to Type-N (m)
|
11903D |
08487-60001 |
|
|
|
Due to the complexity of the PNA family of analyzers, the following notes apply to illustrations in the PNA Help:
|
|
|
The Receiver Compression Above 50 GHz test will also test on the 50 GHz – 67 GHz ports of the test set. |
|
|
Notes for test process on the: N5242A/AS/H85/B, N5244A/AS/B, N5245A/AS/B/BC, N5247A/AS/B/BC
|