|
|
|
This test measures the compression at the specified maximum power level for the receivers, and verifies the Test Port Input – Maximum Test Port Input Level specification, or the Test Port Input – Receiver Compression specification, whichever applies. Compression is measured at various frequencies across the range of the PNA. The test is performed separately on each port, and measures amplitude distortion at the maximum input power level for a given receiver. A negative test result indicates compression while a positive result indicates amplitude expansion.
The test process measures two power deltas, one at the top of the receiver input power range and another in the middle of the input power range. The difference between the two deltas represents the compression at the top of the power range. The PNA provides the signal used to test each port. A cable is used to allow a separate port to drive the port under test. Some PNA models require a Gain Compression Test Set to boost the PNA output to the level required for testing. Some models may require multiple test processes: one for the lower frequency range and another for the upper frequency range.
For troubleshooting help, see Receiver Compression Troubleshooting.
Equipment and connection setups will differ depending on the test plan variant selected: Factory Recommended Variant or Normal Variant. For more information about test plan variants, refer to Test Plan Variants topic.
For a list of required equipment and connection setup illustrations, go to the topic page that matches the test plan variant selected: